Part Number: DRA829V
Hi,
We've received some questions below from my customer. Could you please answer them ?
Let me ask you five questions about ECC.
(1) Does an exception occur when an ECC2bit error occurs?
(2) If an exception does not occur when an ECC2Bit error occurs, is there a way to forcibly generate an exception?
(3) Does an exception occur when an ECC multi 1-bit error occurs?
(4) If an exception does not occur when an ECC multi 1-bit error occurs, is there a way to forcibly generate an exception?
(5) If an ECC multi 1-bit error occurs, will the error information that occurred in two places be accumulated in ① and ② as two error log information?
①DDRSS_ECC_1B_ERR_ADR_LOG_REG (*1)
②DDRSS_ECC_1B_ERR_MSK_LOG_REG (*2)
*1: "4.1.45" in J721E_regisers3.pdf
*2: "4.1.46" in J721E_regisers3.pdf
Regards,
Hideaki