Other Parts Discussed in Thread: TDA4VH
What are the limitations of the camera's online access mode?
How many streams can one VISS access by online and offline mode?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Do you mean OTF (On-The-Fly) mode of VISS? OTF mode can only support single channel per VISS. TDA4VH has two VISS, so can support at max 2 channels in OTF mode.
If 1 channel have accessed to VISS in OTF mode, can this VISS handle other channel in offline mode?
Which psdk version support OTF mode?
Once this VISS is engaged in OTF mode, it cannot be used in memory to memory mode ie offline mode. It can only be used in OTF mode.
As of now, no plan to support OTF mode, due to above limitation.
Regards,
Brijesh
It means VH only support 2 channels access in OTF mode, and no more channels can access even if offline mode. Right?
Yes, that's correct. In VH, if we use OTF mode in VISS, we can support at max 2 cameras/channels in VISS and once they are in OTF, they cannot be used in normal memory to memory mode.