Hi Team,
I am trying to understand which is the recommended flow here for DCC Tuning.
I will tell you the problem first,
I did tuning using DCC tool, create xmls,
Copy that to the sdk folder ti-processor-sdk-rtos-j721e-evm-08_06_01_03/imaging/sensor_drv/src/ar0233/dcc_xmls/wdr ,
Run the ./gUploadenerate_dcc.sh script,
I can see only there binaries here /ti-processor-sdk-rtos-j721e-evm-08_06_01_03/imaging/sensor_drv/src/ar0233/dcc_bins everytime i run this script, i wonder if this is the correct way to do it. Because my changes are not reflecting completely in the Pipeline.
or Should i generate binaries from my dcc tool and directly copy them all to the /ti-processor-sdk-rtos-j721e-evm-08_06_01_03/imaging/sensor_drv/src/ar0233/dcc_bins folder?
Regards,
Dinesh