Part Number: TDA4VM
Hello,
In my model I would like to transpose the output right after the final convolutional layer. It has the shape of BCHW and I would like the transpose it as BHWC.
Unfortunately the TIDL is not supporting the Translate op, but I found that it has a TIDL_ShuffleChannelLayer, described as Reshape + Transpose + Reshape ops in ONNX.
I tried a simple model in torch using a single Conv2d layer and Reshape+Permute+Reshape ops which result exactly with Reshape + Transpose + Reshape ops in ONNX. However the artifacts creation in TIDL still
get the following:
Supported TIDL layer type --- Conv -- Conv_0
Supported TIDL layer type --- Reshape -- Reshape_2
Unsupported (TIDL check) TIDL layer type --- Transpose
Supported TIDL layer type --- Reshape -- Reshape_5
Could you please explain what should be done to exploit the TIDL_ShuffleChannelLayer or suggest another way to perform a Transpose op in TIDL.
Thank you,
Alex.