Part Number: TMS320C6205
Our customer sees C6205 fail to boot on some of their mass-production boards. The C6205 fails to boot when the rise time of the 3.3 V I/O supply is slow (about 10 ms) and succeeds when it is fast. They also confirmed by an A-B-A swap that the issue is not with the board but with C6205.
C6205 does not require specific power sequencing between the core supply and the I/O supply and specific rise time of each power supply, is that correct?
TMS320C6205 Fixed-Point Digital Signal Processor datasheet (Rev. G)
www.ti.com/.../tms320c6205.pdf
power-supply sequencing
"TI DSPs do not require specific power sequencing between the core supply and the I/O supply. However, systems should be designed to ensure that neither supply is powered up for extended periods of time if the other supply is below the proper operating voltage."
The /RESET is pulled-up to the 3.3V I/O supply, not pulled-down, and it is assert after power-up on their boards since the PLL requires a falling edge of /RESET to initialize the PLL engine, is that correct? Not so, it must be pulled-down?
Figure 5. External PLL Circuitry for Either PLL Multiply Modes or x1 (Bypass) Mode
NOTES:
E.
"At power up, the PLL requires a falling edge of RESET to initialize the PLL engine. It may be necessary to toggle reset in order to establish proper PLL operation."
Best regards,
Daisuke