This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

J784S4XEVM: Trace capabilities in Code Composer

Part Number: J784S4XEVM

Hi,

I have previously used the Hardware Trace Analyser & Code Analysis (TVT) with the J721e.  I am unable to use these tools with the J784S4 evaluation board.  The Code Analysis menu is missing the option to start a trace and the Hardware Trace Analyser setup is missing options (e.g. stop on buffer full) and produces an error when started as below.

Is there an issue with my setup or are these features not yet available?

Regards

Stephen