This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Interfacing Ti ADS8365 with TMS320C6747

Other Parts Discussed in Thread: ADS8365

What would be the best way to interface the parallel port AD converter ADS8365 (running at 10MHz clock) with the C6747 (PQFP 176pin version)?

I thought about the Host Port Interface (UHPI) but it seems more complex than what might actually be needed? I don't want to go polling via software if there is a better and more resource saving way of doing things.
Suggestions and links to existing material and documents that might help are greatly appreciated.

Cheers,
Simon.