Part Number: TDA2SX
hi,ti
We will replace the new camera in our recent project. The biggest difference between the new camera and the old camera is that the new camera has 30 frames, while the old camera has 25 frames. After we adapted it, we found the problem shown in the following image, which caused the screen to stutter in the 3D interface. We used the pvrscope command to observe that under the original 25 frame camera, the 3D load rate was around 40%, while under the 30 frame camera, the 3D load rate was around 78%. We suspect that it is due to insufficient GPU performance. GPU frequencies are all 500
We want to solve this problem. Do you have any good optimization suggestions?
thanks,
kong