Part Number: TDA2SX
Hi team,
Using the TDA2XX processor, hang uart3 on A15 (MPU0) using official routine tests. The test is as follows:
1) Data can be received and sent normally using polling.
2) Based on the first point, when a customer reference routine configures the serial port into interrupt mode, the serial port interrupt cannot respond and no data can be received. The interrupt configuration is as follows:
Reference routine:

And made the following modifications:


Could you help check is there anything need to taken care of? Thanks.
Best Regards,
Cherry