Part Number: J721EXCPXEVM
I just received a new J721EXCP01EVM, and I was unable to boot with an SD card using the standard boot configurations. I tested on another EVM with my SD card and it booted just fine. I also switched the J721EX SOM processor board with another one, and it also made no difference. The only difference I noticed on this PCB is that the PCB# PROC079A is the not working one, while the PROC079E3 one was working fine.