Other Parts Discussed in Thread: AM1705, TPS3823, OMAP-L137, AM1707
Hello,
We have built a prototype board using AM1705. We have closely followed the reference design.
We are trying to boot using UART2 of AM1705.
We have set the boot mode to UART2. However we are unable to get "BOOT ME" message on our hyperterminal.
Marking on IC is "AM1705BPTP4: First line; YF - OCAJ4Yw G4: Second Line"
We have even provisioned for secondary reset using TPS3823 supervisory as per errata problem. We have de-coulped WDI pin of TPS3823 IC such that Watchdog functionality is not enabled.
Voltage levels on card are 3.28V (for 3.3V) & 1.18V (for 1.2V)
After reset pin goes high, we observed that TXD2 pin remains high. Does not toggle.
However we have observed that post reset, BOOT12- BOOT14 pins toggle; i.e. BOOT12 is pin multiplexed with EMA_D0/MMCSD_DAT0/GP0_0/BOOT12, EMA_D7/ MMCSD_DAT7/ GP0_7/BOOT13 & EMA_WE/AXR0_12/GP2_3/BOOT14 pins are toggling constantly.
During reset, all boot pins are at correct levels.
We are not sure how to proceed further using UARTx as boot mode.
Kindly suggest what could be the problem.
Kindly revert back at the earliest.
Rgds,
Roma