This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Floating point at OMAP-L137

Hi,

I am a little bit confused about the appropiate configuration and setting for using floating point computations in OMAP L137 (DSP side). When I create a new project I select TMS320C67XX as target, but then in build options I don't know what to select in "Target Version" pop-up menu in the "Basic" category of the "Compiler" tab. I have doubts between C64x+ (-mv6400+) and C67x+ (-mv67p). All examples I have seen up to now always use C64x+ as target version, but none of them are doing floating point compuations. Can you please explain me the difference with these two options and their implications to the performance when mixing both floating point and standard integer operations?

Regards,

Leopoldo.