This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62: what other compatible CAN architectures?

Part Number: SK-AM62
Other Parts Discussed in Thread: CC2640

Hello,

I wanted to know what other compatible CAN architectures  or shared CAN architectures with AM62x?

is any of the below TI platforms shared CAN architecture with AM62x?

AWR Gen1

CC2640

DRA6x (Jacinto5)

DRA7X, TDA2x, TDA3x (Jacinto6)

DRA8x, TDA4x (Jacinto7)

TMS320

TMS470

TMS570

thanks,

Marwan

  • Hello Marwan,

    Please be more specific in what you mean with "CAN architectures".

    How many CANs do you need?

    Does it need to be a specific type of CAN? (e.g., MCAN, DCAN, etc)

    Are the CAN or CANs going to be controlled from a specific core? (e.g., a core running Linux, a real-time core, etc)

    Any other information about your usecase?

    e.g., why are you looking for a processor like AM62x, but not AM62x? Is there a specific feature you are looking for that is not on the AM62x? Did you already do a design with AM62x, and now you are doing a second design with different design constraints? etc.

    Regards,

    Nick

  • Hello Nick,

    Thanks for your response.

    The usecase is about MCAN controlled by R5 or M4 cores, running RTOS.

    The motive for this is that a third party supplier is providing a communication stack solution built on the previously mentioned targets, AM62x is not one of them, so I was wondering if there is a common CAN architecture used between AM62x and any other target, which I can then use its compatible communication stack with AM62x.

    BR,

    Marwan