This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

omapflash get devices ID

As below is omapflash command list:

?OMAPFlash v4.14 (May 12 2011)

usage: omapflash [ <option> ] <command> or omapflash @<file>

OMAP download/upload
  chip_download <device>[@offset] <file>       download file to device starting at offset
  chip_erase <device>[@offset] <size>          erase size bytes (0 is all) in device from offset
  chip_upload <device>[@offset] <size> <file>  upload size bytes to file from device starting at offset

commands (prefixed by command keyword and terminated by newline or comma):
  branch <device> <offset>                     start execution from device and offset address
  jump <absolute address>                      start execution absolute address
  cold_sw_reset                                issue a cold sw reset
  warm_sw_reset                                issue a warm sw reset
  HAL_CM_EnableModuleClocks                    see ROM API function of same name in TRM
  HAL_CTRL_ConfigurePads                       see ROM API function of same name in TRM
  peek32 <address>                             read from memory location
  poke32 <address> <value>                     write to memory location
  peekpoke32 <address> <and value> <or value>  modify memory location

options:
  -com <com port number>                       specify download over UART and com port used
  -usb                                         specify download over USB (default)
  -t <timeout>                                 set communication timeout in seconds
  -p <platform>                                specify the target platform used
  -omap <version>                              specify the OMAP version of the target platform
  -v                                           verbosed output
  @<file>                                      read options/commands form file
                                               use '#' to start comment line
                                               parameters for options/commands must be on same line!

fastboot specific commands:
  fastboot                                     to put OMAPFlash in Fastboot mode
  getvar <variable>                            display a bootloader variable
  flash <partition> [ <file> ]                 write a file to a flash partition
  erase <partition>                            erase a flash partition
  mmcwrite <controller_no> <partition> <file>  write a file to a mmc partition
  mmcerase <controller_no> <partition>         erase a mmc partition
  download <file>                              download an image to memory
  boot <kernel> [ <ramdisk> ]                  download and boot kernel
  reboot                                       reboot device normally
  reboot-bootloader                            reboot device into bootloader

system <command>                               command to execute <command> on host PC

 

There is no way to get Devices id,i try to use omapflash fastboot command,but handset can't boot into bootloader?