In the first contact with this DSP I made different test with the evaluation board DSK6713 and everything was fine. Right now, I've a board desing with a small differences respect to the evaluation board. One of the diference is the sdram memory that i put 256Mbit, 4 blocs, 12 row, 9 col with 32 datas. In one of the datasheets says that this memory is possible to manageted bud when i make the test doesn't work, just work if only make test until 0x10000 address. Some have the solution...
The schematics is identically to the memory of the DSK.
I apreciate your time. thank you in advance
Pere Cárcel