Hi,
In the current bootload process, sbl loads the bootload, and then the bootload loads the app. All three are running on Mcu1_0, and the bootload is loaded to DDR and part of OCMC. When the bootload loads the app from EMMC to DDR, MCU1_0 needs to exit from lockstep mode to split mode, and it will prompt that the operation failed.