This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ipnc_dm365

i want to boot quickly on dm365 with ipnc.but i do not want the net and the audio in the code of ipnc.i only need the video same as the camera.

so can you tell me how to modify the code of ipnc,and do you have these codes like this.

the following is the ipnc module which load in the filesystem.

can you tell me where i can delete.

thx! 

27.339 0.480: CSL: Module install successful, device major num = 253   
27.354 0.016: CSL: Module version 0.10.00, built on Jul 21 2011 21:52:01 
27.964 0.609: I2C: Module install successful, device major num = 252 
27.975 0.011: DMA: Module install successful, device major num = 251 
27.976 0.001: DRV: Module install successful
27.983 0.007: DRV: Module built on Jul 21 2011 21:52:04 
27.985 0.002: DRV: EDMACC.QUEPRI  = 00000777
27.992 0.007: DRV: SYSTEM.MSTPRI0 = 00550011
27.996 0.005: DRV: SYSTEM.MSTPRI1 = 00000444
28.001 0.004: DRV: ISP.BCR        = 00000002
28.377 0.376: CMEMK module: built on Jul 21 2011 at 23:05:55
28.387 0.010:   Reference Linux version 2.6.18
28.403 0.016:   File /nfs/dvsdk_2_10_01_18nuxutils_2_24_02/packages/ti/sdonuxutils/cmem/src/module/cmemk.c
28.839 0.436: ioremap_nocache(0x83c00000, 71303168)=0xc7000000
28.844 0.005: allocated heap buffer 0xc7000000 of size 0x4400000
28.848 0.004: cmem initialized 0 pools between 0x83c00000 and 0x88000000
28.853 0.005: CMEM Range Overlaps Kernel Physical - allowing overlap
28.859 0.006: CMEM phys_start (0x1000) overlaps kernel (0x80000000 -> 0x83c00000)
28.863 0.004: ioremap_nocache(0x1000, 28672)=0xc4068000
28.875 0.012: no remaining memory for heap, no heap created for memory block 1
28.884 0.009: cmem initialized 1 pools between 0x1000 and 0x8000
28.884 0.000: over
29.161 0.277: 
29.164 0.003:  AVSERVER UI: Initializing.
29.164 0.000: 
29.168 0.004: DRV_SyncRst: module = 47, domain = 0, state = 0
29.168 0.000: 
29.173 0.005: DRV_SyncRst: module = 47, domain = 0, state = 3
29.173 0.000:  
29.174 0.001:  CLK Hz,
29.176 0.002:  ARM   Hz =  297000000
29.178 0.002:  DDR   Hz =  243000000
29.180 0.002:  VPSS  Hz =  243000000
29.181 0.001:  IMCOP Hz =  243000000
29.181 0.000:  
29.185 0.003:  DRV LDC: GetConfig 0004 0x0
29.191 0.006: VICP Error: init: Failed to open /dev/irqk: 'No such file or directory'
29.199 0.008: VICP Error: init: Failed to open /dev/irqk: 'No such file or directory'
29.373 0.175:  AVSERVER UI: Starting in mode 6
29.386 0.013:  *** WARNING  FD: exceeded max input size for FD, disabling FD (current input 640x480)!!!
29.429 0.043: DavinciDisplay DavinciDisplay.1: Before finishing with S_FMT:
29.433 0.004: layer.pix_fmt.bytesperline = 640,
29.435 0.003:  layer.pix_fmt.width = 640, 
29.438 0.003:  layer.pix_fmt.height = 480, 
29.441 0.004:  layer.pix_fmt.sizeimage =460800
29.441 0.000: 
29.447 0.006:  Default IconDavinciDisplay DavinciDisplay.1: pixfmt->width = 640,
29.451 0.004:  layer->layer_info.config.line_length= 640
29.451 0.000:  TI Logo
29.453 0.001: 
29.454 0.001:  Default Icon TI Logo
29.456 0.002:  STREAM: Ext 0: 0x0
29.458 0.002:  STREAM: Ext 1: 0x0
29.459 0.001: Creat queue id:0
29.459 0.000: queue id:0
29.586 0.126: IPNC_1.0 (root@localhost.localdomain) (gcc 版本 4.2.0 (MontaV 
29.605 0.019: IPNC AUTO_IRIS = 1 #####################
30.001 0.396:  
30.002 0.001:  Current Settings,
30.005 0.003:  Face Detect                     : OFF
30.010 0.005:  Lens Distortion Correction (LDC): OFF
30.013 0.003:  Video Stabilization             : OFF
30.016 0.003:  SWOSD                           : OFF
30.019 0.003:  Spatial NF                      : OFF
30.023 0.003:  Temporal NF                     : OFF
30.026 0.004:  File Save                       : OFF
30.031 0.004:  AE/AWB                          : OFF
30.036 0.005:  Host-name / IP address          : 192.168.245.111
30.036 0.000: 
30.036 0.001:  ==============
30.038 0.001:  AV Server Main
30.039 0.001:  ==============
30.040 0.001:  
30.042 0.003:  1: Toggle ON/OFF: Face Detect
30.045 0.002:  2: Toggle ON/OFF: LDC
30.048 0.003:  3: Toggle ON/OFF: Video Stabilization
30.052 0.004:  4: Toggle ON/OFF: Spatial  NF
30.055 0.003:  5: Toggle ON/OFF: Temporal NF
30.058 0.003:  6: Toggle ON/OFF: Save to file
30.061 0.003:  7: Toggle ON/OFF: AE/AWB
30.063 0.002:  8: Toggle ON/OFF: SWOSD
30.066 0.004:  b: Enable SWOSD Basic 
30.072 0.005:  d: Enable SWOSD Complete
30.072 0.000:  c: Enable SWOSD Detail 
30.072 0.000:  u: Update SWOSD String 
30.072 0.000:  
30.075 0.003:  r: Save RAW data to file
30.076 0.001:  y: Save YUV data to file
30.079 0.002:  p: Print Profile Info
30.079 0.000:  
30.080 0.001:  0: Stop and Exit
30.081 0.001:  
60.032 29.951:  Enter Choice :