Other Parts Discussed in Thread: SPRC203
C672x Flash access problem
1. We have a C6727 Card with one 16 bit FLASH Am29LV400BB(WORD MODE) WITH
interfaces as per TI (Datasheet-SPRS370,Pg 46, Fig-4.5 & App Note-SPRU711,
Pg 30, Fig-2.9b)
C6727/EM_BA1 TO FLASH/A0
C6727/EM_A0,1,..12 TO FLASH/A1,2,,,13
C6727/GPIO(S) TO FLASH/A14..16
A1CR Reg set for 16 bit EMIF Access
2. Does Anybody have simple routines to access the flash. The routines
which we have from a development board are huge.
3. Is usage of Volatile unsigned short Address necessary ?
4. If I use *p=data or data=*p (with *p as unsigned int) C6727 is writing
32-bit data (2 16-bit data) writes each time and the FLASH write sequence
is getting modified due to 2 writes for each write statement.
Thanks in advance
Rgds
rsp