hello,
I am simply initializing my board.I am using CCS ver 3.1
#include "C:\CCStudio_v3.1\C6000\dsk6416\include\dsk6416.h"
void main()
{
/* Initialize Board Support Library */
DSK6416_init();
}
But receiving this error:
undefined first referenced
symbol in file
--------- ----------------
_MCBSP_open F:\test_interface_DSP\test\test_interface\Debug\main_func.obj
_MCBSP_start F:\test_interface_DSP\test\test_interface\Debug\main_func.obj
_MCBSP_config F:\test_interface_DSP\test\test_interface\Debug\main_func.obj
_DSK6416_init F:\test_interface_DSP\test\test_interface\Debug\main_func.obj
>> error: symbol referencing errors - './Debug/test_interface.out' not built
>> Compilation failure
Build Complete,
2 Errors, 1 Warnings, 0 Remarks.