This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Info about Nand Flash From Micron

Other Parts Discussed in Thread: TMS320DM368

Hi guys i need info about two NAND devices from Micron:

MT29F1G08ABADAH4-IT

MT29F2G08ABAEAH4-IT

I'm planning to replace my old numonyx NAND NAND01GW3B2C with one of the two devices mentioned above.

I tried on my custom board (based on DM368) to use these devices but with no luck. the flash isn't accessible neither with debugger like Lauterbach while with the old Flash everything was fine.

I'm suspecting some troubles occurs during replacing of the chip but i'm not so sure...I need to investigate on these point.

In the meanwhile i'm asking to you guys if someone used successfully these P/N from micron with TMS320DM368 (i need to know if booting from NAND with these devices works fine!

thank you all!