Hi All,
I have a question, we use OMAP-L138 chip in our HW and currently we have new HW version with crystal 27 MHz
I knew that the UBL we have supporting 24 MHz so I need to change the UBL in order to support 27 MHz crystal instead of 24 MHz.
My question is, as it seems there is two steps to make that :
1 - Build the UBL itself and produce *.out
2 - Use the AISGen tool to produce *.bin
to Make the needed change, Is it enough to change the settings of the AIS gen tool , or there is something needed to change in (1) ?