This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: Disable MAIN_UART1 in TIFS firmware

Part Number: AM625

Hi,

Customer wants to use MAIN_UART1 in application. How to disable MAIN_UART1 in TIFS firmware?

  • Hi Nancy,

    Please apply the following patch to the SDK board-support/k3-image-gen-2022.01/, then rebuild u-boot. This should prevent TIFS using MAIN_UART1.

    --- soc/am62x/evm/board-cfg.c.orig      2023-06-30 09:17:09.910434836 -0500
    +++ soc/am62x/evm/board-cfg.c   2023-06-30 09:18:07.096173838 -0500
    @@ -78,7 +78,7 @@
                            .size = sizeof(struct boardcfg_dbg_cfg),
                    },
     #ifdef ENABLE_TRACE
    -               .trace_dst_enables = BOARDCFG_TRACE_DST_UART0 |
    +               .trace_dst_enables =
                                         BOARDCFG_TRACE_DST_ITM |
                                         BOARDCFG_TRACE_DST_MEM,
                    .trace_src_enables = BOARDCFG_TRACE_SRC_PM |