Other Parts Discussed in Thread: TDA4VM
We are trying to enable a GPIO0_64 and get the User LED LD2 of TDA4VM edge AI Kit(PROC112A(001)) powered up.
- We have written the PadConfig PRG0_PRU0_GPO1@ 0x0011c0b4 with the value 00060007.
- Set the direction at 0x00600060 from 0xff79ff3f to 0xff79ff3e.
- We have also set ICSSG_GPCFG0_REG at 0x0B026008 to enable GPIO mux.
- We can see the status changing at 0x00600064 when setting and clearing the bits at 00600068 and 0060006C, but it is not getting reflected.(LED is still off)
- We have verified the register values after booting using the k3conf app as well.
Are we missing something, any pointers are welcome.
NB: This is done in QNX startup, hw_init.c.
Regards,
Neeraj