Part Number: AM6442
Hi all
Would you mind if we ask some questions about AM6442 memory address?
<Question1>
In TRM 4.8.1 Memory Layout/MPU, We think ROM code address is Region 1.
And (If OSPI boot) SBL address in OSPI memory is Region 11.
Is our recognition correct?
<Question2>
In the memory layout, and if we select another boot device in ROM code (e.g. eMMC, GPMC, I2C, USB..), which region will executable as SBL?--
<Question3>
If we use sbl_prebuilt/am64x-evm/sbl_ospi.release.hs_fs.tiimage, will software image execute on address 0x60080000?
Is the offset SBL space?
And is offset defined by SBL's linker command file?
Kind regards,
Hirotaka Matsumoto