This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VH-Q1: When downloading programs or debugging video ISPs, you must use USB3.0. Is it possible not to use the USB3.0 interface,

Part Number: TDA4VH-Q1


  • 下载程序或者视频ISP调试的时候,是否一定要使用USB3.0。是否可以不使用USB3.0接口,
  • When downloading programs or debugging video ISPs, you must use USB3.0. Is it possible not to use the USB3.0 interface,