This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-J721S2: linux 8.5

Part Number: PROCESSOR-SDK-J721S2


hello ti

    when we debug A72, at the startup stage, serial gives us following error

NOTICE: BL31: v2.7(release):v2.7.0-359-g1309c6c80-dirty
NOTICE: BL31: Built : 13:08:29, Jun 29 2023
I/TC:
I/TC: OP-TEE version: 3.19.0-dev (gcc version 9.2.1 20191025 (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10))) #16 Mon Jul 3 08:25:41 UTC 2023 aarch64
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check optee.readthedocs.io/.../porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.3--v08.06.03 (Chill Capybar')
I/TC: HUK Initialized
I/TC: 1111111111111111111111111111111111 SA2UL_TI_SCI_DEV_ID = 297
E/TC:0 0 k3_sec_proxy_verify_thread:108 Queue is busy
E/TC:0 0 k3_sec_proxy_recv:196 Thread SEC_PROXY_RESPONSE_THREAD verification failed. ret = -65523
E/TC:0 0 ti_sci_get_response:101 Message receive failed (-65523)
E/TC:0 0 ti_sci_do_xfer:150 Failed to get response (-65523)
E/TC:0 0 sa2ul_init:60 Failed to get SA2UL device
E/TC:0 0 call_initcalls:43 Initcall __text_start + 0x0005c898 failed
I/TC: Primary CPU switching to normal world boot

    According to our check, the control flow has reached following place

    but it returns from smc.

    so could you please tell me where control flow go, what code will execute when code executes smc #0 next. Thanks