This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ccs 2.2 to 3.3 migration issues



I have a older project that I wanted to upgrade to the newest ccs.  It migrated over fine (I added the cslCfgInit() to the main and such).  My only problem that I was taking up a bit too much memory (6711 running out of intmem), but disabling the "use Instrumented Bios library" and "Real Time Analysis" freed up enough memory.

The problem I am having is that the program appears to run into the weeds and crash CCS just after the start of the program, not even getting to main. 

 

Right now I'm looking into the memory.  What does Copy Section mean in memory?  When I load my program via the emulator does it not load that?  In my example below .vers, .hwi_vec, and $BRID  all start at 0x00000000

 

MEMORY CONFIGURATION

         name            origin    length      used     unused   attr    fill
----------------------  --------  ---------  --------  --------  ----  --------
  IntMem                00000000   0000fe58  0000f2ad  00000bab  RWIX
  ad_stat_init_sec      0000fe58   00000004  00000004  00000000  RWIX
  sband_sec             0000fe5c   00000004  00000004  00000000  RWIX
  hpi_tx_buffer         0000fe60   00000190  00000000  00000190  RWIX
  ArgSec                0000fff0   00000010  00000004  0000000c  RWIX
  SDRAM                 80000000   01000000  0036a720  00c958e0  RWIX
  dsp2_hpi_reg          90000000   00000020  00000020  00000000  RWIX
  cpld1controlblock     b0000000   00000100  00000018  000000e8  RWIX


SECTION ALLOCATION MAP

 output                                  attributes/
section   page    origin      length       input sections
--------  ----  ----------  ----------   ----------------
.vers      0    00000000    00000040     COPY SECTION
                  00000000    00000040     Ts1_Dsp1cfg.obj (.vers)

.hwi_vec   0    00000000    00000200    
                  00000000    00000200     Ts1_Dsp1cfg.obj (.hwi_vec)

.pinit     0    00000000    00000000     UNINITIALIZED

.trace     0    00000000    00000000    

.pip       0    00000000    00000000     UNINITIALIZED

.stack     0    00000000    00000000     UNINITIALIZED

$BRID      0    00000000    000001a0     COPY SECTION
                  00000000    000000b4     csl6711.lib : csl_edma.obj ($BRID)
                  000000b4    00000078                 : csl_irq.obj ($BRID)
                  0000012c    00000060                 : csl_timer.obj ($BRID)
                  0000018c    00000014                 : csl.obj ($BRID)

.text      0    00000200    000073a0    

 

 

 

Thanks

Bryce