This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM648 video port can't receive Cb and Cr ,but can receive Y



 Hello,

Everyone.I'm doing with Lyrtech's DVDP648.I want to use video port 3 to capture BT.656 576x704 interlaced video.I can receive Y

signal correctly,but can not receive Cb and Cr signal.I link the EDMA PaRam-Set to null-PaRam-Set  when a frame is completed.I go

to see the EDMA registers window with CCS,I can find that only the Y-signal  corresponding PaRam-Set is null-PaRam-Set ,but Cb

and Cr corresponding PaRam-Set don't link to null-PaRam-Set ,and I can find only 2 double words of Cb and Cr data have been

transfered from the DST entry of the OPT i of the corresponding PaRam-Set .And I can find there was no event missing from EMR and

EMRH regesters in EDMA.It implys that only two VPCbEVTA and VPCrEVTA  event signal generated. I can also find the value of VPIS

register in VP3 is 0x00000006,and this implys video capture have completed and there was FIFO overruned. So it's complicated and

I can't find where the problem is.

the following is some setup parameters with video port and EDMA.

/***************************************** VIDEO PORT SETUP***************************************/

#define PORTPARAM {\
 /* //以下通过VPCTL寄存器设置                             */\
 /*                                                           */\
 /*  //设置作为视频捕获还是视频显示,0:capture 1:display          */\
 0,/*                                                         */\
 /*  //双通道还是单通道,0:single channel 1:dual channel                */\
 0,/*  //dual channel                                         */\
 /*  //VPXCLK1极性是否翻转,只用于视频显示口 1:翻转 (inverse)         */\
 0,/*                                                         */\
 /*  //VPxCTL0,1, 2极性设置 0:高有效(active high) 1:低有效(active low) */\
 0,0,0/*                                                    */\
 }

/*********************************************CAPTURE PORT SETUP***************************************/
 #define CAPPARAM {\
 /* //VCACTL,VCBCTL                                        */\
 /*  //capture mode select 0:8-bit BT.656                                   */\
 /*  //   2:8-bit raw                                     */\
 /*  //   4:16-bit Y/C                                    */\
 /*  //   6:16-bit raw                                    */\
 0,/*  //Uint8 cmode;                                          */\
 /*  //操作模式选择,CON,FRAME,CF2,CF1                        */\
 /*  //1:Noncontinuous field 1 capture                        */\
 /*  //2:Noncontinuous field 2 capture                        */\
 /*  //3:Noncontinuous field 1 and field 2 capture            */\
 /*  //4:Noncontinuous frame capture                          */\
 /*  //5:Noncontinuous progressive frame capture              */\
 /*  //7:Single frame capture                                 */\
 /* //9:Continuous field 1 capture            */\
 /*  //10:Continuous field 2 capture              */\
 /*  //12:Continuous frame capture.               */\
 /*  //13:Continuous progressive frame capture  */\
 7,/*  //Uint8 cfcc;//CON,FRAME,CF2,CF1                       */\
 /*  //scaling,0:no,1:1/2 scaling                               */\
 0,/*  //Uint8 scale;                                          */\
 /*  //resampling,0:no 1:yes                                 */\
 0,/*  //Uint8 resmpl;                                         */\
 /*  //HCOUNT VCOUNT reset method,field detect method          */\
 1,0,0,/*  //Uint8 hrst,vrst,fldd;                             */\
 /*  //选择用同步信号,还是EAV/SAV 0:用EAV、SAV 1:用同步信号  */\
 0,/*  //Uint8 exc;                                            */\
 /*  //F位。。。0:Detected 0 is field 1.                       */\
 /*  //   1:Detected 0 is field 2.                      */\
 1,/*  //Uint8 finv;                                           */\
 /*                                                            */\
 /*  //VCxSTRT1,场1图像起始位置,x代表A或B                     */\
 0,25,/*  //Uint16 vcxstart1,vcystart1;//vcxstart必须是偶数  */\
 /*                                                            */\
 /*  //VCxSTOP1,场1图像终止位置                                */\
 704,312,/*  //Uint16 vcxstop1,vcystop1;                       */\
 /*                                                            */\
 /*  //VCxSTRT2,场2图像起始位置,x代表A或B                     */\
 0,26,/*  //Uint16 vcxstart2,vcystart2;//vcxstart必须是偶数 */\
 /*                                                            */\
 /*  //VCxSTOP2,场2图像终止位置                                */\
 704,313,/*860,313,  //Uint16 vcxstop2,vcystop2;                       */\
 /*                                                            */\
 /*  //VCxTHRLD,阈值                                           */\
 88,88,/*88,88,  //Uint16 vcthrld1,vcthrld2;//只有10位               */\
 /*                                                            */\
 /*  //VCxEVTCT,设置每场的事件数                               */\
 288,288/*  //Uint16 capevtct1,capevtct2;                      */\
 }

/**************************************************Y PARAM-SET***********************************************/
#define EDMAPARAMY_FLD1 {\
  /* //传输通道                                                    */\
  38,/*  Uint8 chan;                                                      */\
  /*//传输队列,也就是TC0~TC3,0的优先级最高,3的优先级最低  */\
  1,/*Uint8 queue;             */\
  /*  //传输所用参数集                                                 */\
  38,/*  Uint16 paramsetnum;                                              */\
  /*  //paramset                                                       */\
  /*  //opt                                                            */\
  /*  //Source/Destination address mode.                               */\
  /*  //0:Increment (INCR) mode                                        */\
  /*  //1:Constant addressing (CONST) mode                             */\
  0,/*  0,Uint8 sam;                                                       */\
  0,/*  Uint8 dam;                                                       */\
  /*  //传输同步方式,0:A-synchronized 1:AB-synchronized.               */\
  1,/*1,  Uint8 syncdim;                                                   */\
  /*  //Static set.0:Set is not static 1: Set is static                */\
  0,/*  Uint8 static_;                                                   */\
  /*  //FIFO Width 0:8-bit 1:16-bit 2:32-bit 3:64-bit 4:128-bit
      */\
  /*  //5:256-bit                                                      */\
  0,/* 0, Uint8 fwid;                                                      */\
  /*  //Transfer complete code mode.                                   */\
  /*  //0:Normal completion: A transfer is considered completed
      */\
  /*  //after the data has been transferred.                           */\
  /*  //1:Early completion: A transfer is considered completed after
 */\
  /*  //the EDMA3CC submits a TR                                       */\
  0,/*  Uint8 tccmode;                                                   */\
  /*  //Transfer complete code.6位二进制,0-0x3F                        */\
  38,/*  Uint8 tcc;                                                       */\
  /*  //Transfer complete/Intermediate transfer completion interrupt
 */\
  /*  //enable.                                                        */\
  /*  //0:Transfer complete interrupt is disabled.                     */\
  /*  //1:Transfer complete interrupt is enabled.                      */\
  0,/*  Uint8 tcinten;                                                   */\
  0,/*  Uint8 itcinten;                                                  */\
  /*  //Transfer complete/Intermediate transfer completion chaining
  */\
  /*  //enable.                                                        */\
  /*  //0:Transfer complete chaining is disabled.                      */\
  /*  //1:Transfer complete chaining is enabled.                       */\
  0,/*  Uint8 tcchen;                                                    */\
  0,/*  Uint8 itccen;                                                    */\
  /*  //Channel Source Address (SRC)                                   */\
  CSL_VP3_CHANNELA_DATA,/*  Uint32 src;                                                      */\
  /*  //Channel Destination Address (DST)                              */\
  0,/*  Uint32 dst;                                                      */\
  /*  //Count for 1st Dimension (ACNT)                                 */\
  8, /*704, Uint16 acnt;                                                     */\
  /*  //Count for 2nd Dimension (BCNT)                                 */\
  88, /*576, Uint16 bcnt;                                                     */\
  /*  //Count for 3rd Dimension (CCNT)                                 */\
  576,/*1,  Uint16 ccnt;                                                     */\
  /*  //BCNT Reload (BCNTRLD)                                          */\
  0,/*576,  Uint16 bcntrld;                                                  */\
  /*  //Source B Index (SRCBIDX)                                       */\
  0,/*  Int16 srcbidx;                                                   */\
  /*  //Destination B Index (DSTBIDX)                                  */\
  8,/*704,1408,  Int16 dstbidx;                                                   */\
  /*  //Source C Index (SRCCIDX)                                       */\
  0,/*  Int16 srccidx;                                                   */\
  /*  //Destination C Index (DSTCIDX)                                  */\
  704,/* 0, Int16 dstcidx;                                                   */\
  /*  //Link Address (LINK),aligned 32-byte,The 5 LSBs of the LINK
   */\
  /*  //field should be cleared to 0.                                  */\
  /*  //The EDMA3CC ignores the upper 2 bits of the LINK entry         */\
  0xffff/* (38+64)<<5 Int16 link;38+64                                                      */\
 }

/**************************************************Cb PARAM-SET***********************************************/
#define EDMAPARAMCb_FLD1 {\
  /* //传输通道                                                    */\
  39,/*  Uint8 chan;                                                      */\
  /*//传输队列,也就是TC0~TC3,0的优先级最高,3的优先级最低  */\
  0,/*Uint8 queue;             */\
  /*  //传输所用参数集                                                 */\
  39,/*  Uint16 paramsetnum;                                              */\
  /*  //paramset                                                       */\
  /*  //opt                                                            */\
  /*  //Source/Destination address mode.                               */\
  /*  //0:Increment (INCR) mode                                        */\
  /*  //1:Constant addressing (CONST) mode                             */\
  0,/*  Uint8 sam;                                                       */\
  0,/*  Uint8 dam;                                                       */\
  /*  //传输同步方式,0:A-synchronized 1:AB-synchronized.               */\
  0,/*  Uint8 syncdim;                                                   */\
  /*  //Static set.0:Set is not static 1: Set is static                */\
  0,/*  Uint8 static_;                                                   */\
  /*  //FIFO Width 0:8-bit 1:16-bit 2:32-bit 3:64-bit 4:128-bit
      */\
  /*  //5:256-bit                                                      */\
  0,/*  Uint8 fwid;                                                      */\
  /*  //Transfer complete code mode.                                   */\
  /*  //0:Normal completion: A transfer is considered completed
      */\
  /*  //after the data has been transferred.                           */\
  /*  //1:Early completion: A transfer is considered completed after
 */\
  /*  //the EDMA3CC submits a TR                                       */\
  0,/*  Uint8 tccmode;                                                   */\
  /*  //Transfer complete code.6位二进制,0-0x3F                        */\
  39,/*  Uint8 tcc;                                                       */\
  /*  //Transfer complete/Intermediate transfer completion interrupt
 */\
  /*  //enable.                                                        */\
  /*  //0:Transfer complete interrupt is disabled.                     */\
  /*  //1:Transfer complete interrupt is enabled.                      */\
  0,/*  Uint8 tcinten;                                                   */\
  0,/*  Uint8 itcinten;                                                  */\
  /*  //Transfer complete/Intermediate transfer completion chaining
  */\
  /*  //enable.                                                        */\
  /*  //0:Transfer complete chaining is disabled.                      */\
  /*  //1:Transfer complete chaining is enabled.                       */\
  0,/*  Uint8 tcchen;                                                    */\
  0,/*  Uint8 itccen;                                                    */\
  /*  //Channel Source Address (SRC)                                   */\
  CSL_VP3_CHANNELA_DATA+0x20,/*  Uint32 src;                                                      */\
  /*  //Channel Destination Address (DST)                              */\
  0,/*  Uint32 dst;                                                      */\
  /*  //Count for 1st Dimension (ACNT)                                 */\
  8,/*  Uint16 acnt;                                                     */\
  /*  //Count for 2nd Dimension (BCNT)                                 */\
  44,/*576,  Uint16 bcnt;                                                     */\
  /*  //Count for 3rd Dimension (CCNT)                                 */\
  576,/*1,  Uint16 ccnt;                                                     */\
  /*  //BCNT Reload (BCNTRLD)                                          */\
  0,/*576,  Uint16 bcntrld;                                                  */\
  /*  //Source B Index (SRCBIDX)                                       */\
  0,/*  Int16 srcbidx;                                                   */\
  /*  //Destination B Index (DSTBIDX)                                  */\
  8,/*352, 704 Int16 dstbidx;                                                   */\
  /*  //Source C Index (SRCCIDX)                                       */\
  0,/*  Int16 srccidx;                                                   */\
  /*  //Destination C Index (DSTCIDX)                                  */\
  352,/*0,  Int16 dstcidx;                                                   */\
  /*  //Link Address (LINK),aligned 32-byte,The 5 LSBs of the LINK
   */\
  /*  //field should be cleared to 0.                                  */\
  /*  //The EDMA3CC ignores the upper 2 bits of the LINK entry         */\
  0xffff/*(39+64)<<5  Int16 link;39+64                                                      */\
 }


/**************************************************Cr PARAM-SET***********************************************/

#define EDMAPARAMCr_FLD1 {\
  /* //传输通道                                                    */\
  40,/*  Uint8 chan;                                                      */\
  /*//传输队列,也就是TC0~TC3,0的优先级最高,3的优先级最低  */\
  0,/*Uint8 queue;             */\
  /*  //传输所用参数集                                                 */\
  40,/*  Uint16 paramsetnum;                                              */\
  /*  //paramset                                                       */\
  /*  //opt                                                            */\
  /*  //Source/Destination address mode.                               */\
  /*  //0:Increment (INCR) mode                                        */\
  /*  //1:Constant addressing (CONST) mode                             */\
  0,/*  Uint8 sam;                                                       */\
  0,/*  Uint8 dam;                                                       */\
  /*  //传输同步方式,0:A-synchronized 1:AB-synchronized.               */\
  0,/*  Uint8 syncdim;                                                   */\
  /*  //Static set.0:Set is not static 1: Set is static                */\
  0,/*  Uint8 static_;                                                   */\
  /*  //FIFO Width 0:8-bit 1:16-bit 2:32-bit 3:64-bit 4:128-bit
      */\
  /*  //5:256-bit                                                      */\
  0,/*  Uint8 fwid;                                                      */\
  /*  //Transfer complete code mode.                                   */\
  /*  //0:Normal completion: A transfer is considered completed
      */\
  /*  //after the data has been transferred.                           */\
  /*  //1:Early completion: A transfer is considered completed after
 */\
  /*  //the EDMA3CC submits a TR                                       */\
  0,/*  Uint8 tccmode;                                                   */\
  /*  //Transfer complete code.6位二进制,0-0x3F                        */\
  40,/*  Uint8 tcc;                                                       */\
  /*  //Transfer complete/Intermediate transfer completion interrupt
 */\
  /*  //enable.                                                        */\
  /*  //0:Transfer complete interrupt is disabled.                     */\
  /*  //1:Transfer complete interrupt is enabled.                      */\
  0,/*  Uint8 tcinten;                                                   */\
  0,/*  Uint8 itcinten;                                                  */\
  /*  //Transfer complete/Intermediate transfer completion chaining
  */\
  /*  //enable.                                                        */\
  /*  //0:Transfer complete chaining is disabled.                      */\
  /*  //1:Transfer complete chaining is enabled.                       */\
  0,/*  Uint8 tcchen;                                                    */\
  0,/*  Uint8 itccen;                                                    */\
  /*  //Channel Source Address (SRC)                                   */\
  CSL_VP3_CHANNELA_DATA+0x40,/*  Uint32 src;                                                      */\
  /*  //Channel Destination Address (DST)                              */\
  0,/*  Uint32 dst;                                                      */\
  /*  //Count for 1st Dimension (ACNT)                                 */\
  8,/*352,  Uint16 acnt;                                                     */\
  /*  //Count for 2nd Dimension (BCNT)                                 */\
  44,/*576,  Uint16 bcnt;                                                     */\
  /*  //Count for 3rd Dimension (CCNT)                                 */\
  576,/*  Uint16 ccnt;                                                     */\
  /*  //BCNT Reload (BCNTRLD)                                          */\
  0,/*576,  Uint16 bcntrld;                                                  */\
  /*  //Source B Index (SRCBIDX)                                       */\
  0,/*  Int16 srcbidx;                                                   */\
  /*  //Destination B Index (DSTBIDX)                                  */\
  8,/*352,  Int16 dstbidx;                                                   */\
  /*  //Source C Index (SRCCIDX)                                       */\
  0,/*  Int16 srccidx;                                                   */\
  /*  //Destination C Index (DSTCIDX)                                  */\
  352,/*0,  Int16 dstcidx;                                                   */\
  /*  //Link Address (LINK),aligned 32-byte,The 5 LSBs of the LINK
   */\
  /*  //field should be cleared to 0.                                  */\
  /*  //The EDMA3CC ignores the upper 2 bits of the LINK entry         */\
  0xffff/*(40+64)<<5  Int16 link;40+64                                                      */\
 }