Hello,
I trying to boot a Sys/BIOS application from the NOR flash on the C6678 EVM, but with no success.
I already booted the nor boot example and the post example.
Now I compiled the BIOS Hello world template an made it write to the UART, but no matter what I try to do it doesn't work.
I tried to use the hex6x with the -boot parameter and it also faild.
It seems like I missing a parameter in the linker configuration?
Thanks,
Jim