Part Number: J721EXSOMXEVM
1 Can the GP of your TI EVM official board J721EXSOMG01EVM run the secure encryption HSM module? Or does it have to be HS?
2 I ran vector's autosar secure encryption HSM on the GP version of the EVM official board J721EXSOMG01EVM. When I run the HOST end on the R5F core of the mcu and the HSM end on the Cortex-M3 core, I can load the run separately. However, when I run at the same time, the ccs debugger single-step HOST code will run around and cannot run normally single-step.