This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6713 and MMC/SD



Hi all

I need to connect the MMC/SD to the C6713 using spectrumdigial DSK6713 I have some questions :

1) C6713 has no CSL functions to support the MMC/SD, is there any new library added to supporting the MMC/CD like TI c5509;
Is there any specific application note to C6713 to driving the MMC/SD card using the MCBSP channel.

2)Is there any free library to driving MMC/CD to File system in MMC/SD in C6713
 
3)C6713 has two MCBSP channel   which can be configured in SPI mode. The "SpectrumDigital" DSK6713  used one of the MCBSP channels to communicate AI23 during the configuring this chip, Is possible in the Same time I used this used channel with the Other device like another codec or MMC/SD card without any additional channel for CS(chip select) or FS signal.

Best regards