Other Parts Discussed in Thread: TMS320C6416
Hi,
I was wondering if anyone can recommend a DSP kit suitable for an object recognition system.
I need to be able to program it with MATLAB such as can be done with the TMS320C6416 DSP Starter Kit,
Also are there camera modules which can be connected to the TMS320C6416 or a kit which has a camera included
i only need a resolution of 640x480, frame rate >10fps.
Thanks for any replies!