Hi TI Support team,
I'd like to have a question.
My team observe that the output build from SDK and the Yocto are different.
For examble:
The Linux kernel:
- Build from SDK: We have the error relate to "cryptodev" and it lead to the issue that IPC is not working:

- Built from Yocto: The built output is normall, there are no issue about cryptodev and IPC working normally.
Uboot:
We just found that the Uboot from Yocto and SDK also have different boot arguments.
We are using the SDK from here: https://www.ti.com/tool/download/PROCESSOR-SDK-LINUX-J721E/08.05.00.08
May I ask why there are different between them even the source code are the same? May I missed some steps during the environment setup?
Best regards,
Loc.Ta.