Part Number: AM5748
Which version of CCS is needed to program both DSP and ARM on AM5748? Which CCS version has the necessary PDK, compiler etc needed for AM5748 along with its installation?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM5748
Which version of CCS is needed to program both DSP and ARM on AM5748? Which CCS version has the necessary PDK, compiler etc needed for AM5748 along with its installation?
Hi Ashok,
You can check the CCS version being used in pdkProjectCreate.bat file at <PDK>/packages path. You can use that version to work with the given PDK package.
Regards,
Parth
I am trying to download and install pdk from this location:
https://www.ti.com/tool/PROCESSOR-SDK-AM57X
But the windows installer file after downloading successfully, gives errors during extracting. tried multiple times, but the same issue is coming. Any inputs on this..?
Hi,
Can you please mention what error you are seeing?
Maybe you can share the screenshot of the issue?
Regards,
Parth
Hi Ashok,
This should not be an issue, you should still be able to use SDK without issues.
Regards,
Parth