So if designing LPDDR4 the second rank (DDR0_CS1_N) cannot be used ? If so was it usable in the regular DDR4 component ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
So if designing LPDDR4 the second rank (DDR0_CS1_N) cannot be used ? If so was it usable in the regular DDR4 component ?
Greetings Huynh,
I'm not sure exactly what you're asking, can you clarify if you are asking about the different addressing options between DDR4 and LPDDR4?
Sincerely,
Lucas
Thank you for clarification. So the next question is what is the use or purpose of DDR0_CS1_N? Is it something for future expansion or is it possible we use 2 devices (for 2 separate chip selects) of single rank LPDDR4/DDR4 ?
Also I need the explanation of the AM64xx TRM section 8.1.1 (DRSS Overview) where it said Memory Bus Features of up to 2 ranks and SDRAM address range up to 8GB. But the section 8.1.1.1 (DDRSS Not Supported Features) indicated : only 1 rank design is supported and up to 2GB dram space. So what is the purpose of the feature set in 8.1.1.
Thanks,
Huynh
Huynh, the DDR IP supports dual rank, but we deprecated that feature in AM64x, so this pin is not used. It may be enabled in the future, but most likely it will not as signal rank 2GB devices are easily available.
The feature set in 8.1.1 describes the DDR IP feature set, some of which can be deprecated as described in the Not Supported Features section
Regards,
James