Part Number: AM4376
Hi team,
Our customer is developing the next generation system with AM4376BZDNA100, and customer is performing EMC test (Radiated emissions test). According to the requirement of Emission standard spec, it seems the maximum of measurement frequency is 5GHz when The highest frequency used inside the system is 1GHz. So, customer is asking question about the highest frequency processing speed inside AM4376.
If customer is configured Cortex-A9 to “Nitro mode”, Cortex-A9 is working at 1GHz. I believe this frequency speed(1GHz) is highest one inside AM4376. Is that correct? If there is more higher frequency signals, would you clarify this frequency value, please?
I really appreciate if you will share your advice/comments on this inquiry.
Best regards,
Miyazaki