Hi Judith,
we are able to successfully download U-boot images and tisdk-base.ext4
and we send the following commands to boot from eMMC
=> setenv mmcdev 0
=> setenv bootpart 0
power off the device, changed boot mode switches to eMMC boot. we get following error.
U-Boot SPL 2021.01-00002-g93da3fa57b (Jul 03 2023 - 10:27:32 +0530)
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar')
SPL initial stack usage: 13424 bytes
Trying to boot from MMC1
spl: could not initialize mmc. error: -19
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###.
attaching log file from target.
U-Boot SPL 2021.01-00002-g93da3fa57b (Jul 03 2023 - 10:27:32 +0530)
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar')
SPL initial stack usage: 13424 bytes
Trying to boot from DFU
###############################################DOWNLOAD ... OK
Ctrl+C to exit ...
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Loading Environment from MMC... MMC Device 0 not found
*** Warning - No MMC card found, using default environment
init_env from device 10 not supported!
Starting ATF on ARM64 core...
NOTICE: BL31: v2.8(release):v2.8-226-g2fcd408bb3-dirty
NOTICE: BL31: Built : 05:06:58, Feb 24 2023
U-Boot SPL 2021.01-00002-g93da3fa57b (Jul 03 2023 - 10:27:08 +0530)
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar')
Trying to boot from DFU
####DOWNLOAD ... OK
Ctrl+C to exit ...
U-Boot 2021.01-00002-g93da3fa57b (Jul 03 2023 - 10:27:08 +0530)
SoC: AM62X SR1.0 GP
Model: Texas Instruments AM625 SK
EEPROM not available at 0x50, trying to read at 0x51
Board: AM62-SKEVM rev E3
DRAM: 2 GiB
MMC: mmc@fa10000: 0, mmc@fa00000: 1, mmc@fa20000: 2
Loading Environment from MMC... OK
In: serial@2800000
Out: serial@2800000
Err: serial@2800000
Net: eth0: ethernet@8000000port@1
Hit any key to stop autoboot: 0
=>
=>
=> env default -f -a
## Resetting to default environment
=> pri dfu_alt_info_emmc
dfu_alt_info_emmc=rawemmc raw 0 0x800000 mmcpart 1;rootfs part 0 1 mmcpart 0;tiboot3.bin.raw raw 0x0 0x400 mmcpart 1;tispl.bin.raw raw 0x400 0x1000 mmcpart 1;u-boot.img.raw raw 0x1400 0x2000 mmcpart 1;u-env.raw raw 0x3400 0x100 mmcpart 1;sysfw.itb.raw raw 0x3600 0x800 mmcpart 1
=> editenv dfu_alt_info_emmc
edit: rawemmc raw 0 0x800000 mmcpart 1;rootfs part 0 1 mmcpart 0;tiboot3.bin.raw raw 0x0 0x400 mmcpart 1;tispl.bin.raw raw 0x400 0x1000 mmcpart 1;u-boot.img.raw raw 0x1400 0x2000 mmcpart 1;u-env.raw raw 0x3400 0x100 mmcpart 1;sysfw.itb.raw raw 0x3600 0x800 mmcpart 1
=> pri dfu_alt_info_emmc
dfu_alt_info_emmc=rawemmc raw 0 0x800000 mmcpart 1;rootfs part 0 1 mmcpart 0;tiboot3.bin.raw raw 0x0 0x400 mmcpart 1;tispl.bin.raw raw 0x400 0x1000 mmcpart 1;u-boot.img.raw raw 0x1400 0x2000 mmcpart 1;u-env.raw raw 0x3400 0x100 mmcpart 1;sysfw.itb.raw raw 0x3600 0x800 mmcpart 1
=> setenv dfu_alt_info ${dfu_alt_info_emmc}
=> pri dfu_alt_info
dfu_alt_info=rawemmc raw 0 0x800000 mmcpart 1;rootfs part 0 1 mmcpart 0;tiboot3.bin.raw raw 0x0 0x400 mmcpart 1;tispl.bin.raw raw 0x400 0x1000 mmcpart 1;u-boot.img.raw raw 0x1400 0x2000 mmcpart 1;u-env.raw raw 0x3400 0x100 mmcpart 1;sysfw.itb.raw raw 0x3600 0x800 mmcpart 1
=> dfu 0 mmc 0
##DOWNLOAD ... OK
Ctrl+C to exit ...
####DOWNLOAD ... OK
Ctrl+C to exit ...
####DOWNLOAD ... OK
Ctrl+C to exit ...
################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################################DOWNLOAD ... OK
Ctrl+C to exit ...
=> setenv mmcdev 0
=> setenv bootpart 0
=> ð
U-Boot SPL 2021.01-00002-g93da3fa57b (Jul 03 2023 - 10:27:32 +0530)
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar')
SPL initial stack usage: 13424 bytes
Trying to boot from MMC1
spl: could not initialize mmc. error: -19
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###
please help us in fixing the issue.
Thanks and Regards,
Swapna.