Part Number: AM6442
Other Parts Discussed in Thread: AM5726
Hello,
we have develloped a smart camera based on the AM5726 and our own camera module and for the future we would like to use an AM6xxx
processor to make use of a platform. As we spend a lot of development effort into the image interface for real time features we are
searching for a processor from the AM6xxx family which can be used with our existing camera module.
Our current smart camera consists of an AM5726 and our own camera module with an image sensor and an fpga.
The fpga converts the image so that we have a frame valid, line valid, pixel clock and 16 bits in parallel at the video input port.
On the AM5726 we use VIP3 to capture 16bpp grayscale images. The pixel clock is generated by the fpga and it is at a maximum of around 125MHz.
Our requirements for the new processor are:
1. Video-/Image- input port with 16bit parallel data input for 16bit per pixel, frame valid and pixel clock (line valid might be not necessary)
2. Pixel clock is generated by the fpga
3. Pixel clock up to 125HHz
In the future we would like to use an AM6xxx Processor. I saw that some AM64xx Processors have a MIPI CSI-2 Interface but using this
would mean that we have to spend a lot of effort to redesign our camera module. So my questions are:
1. Is it possible to implement an image interface on a PRU?
2. Are there examples for using a PRU for that in an SDK ore somewhere else?
3. I unsed the TI-Sysconfig tool an saw that there is a Pin Configuration for 16 bit parallel data input with the PRU. Is there an EVM
with an AM64xx processor where these data lines are on a socket so that I can connect our camera module?
Thank you very much.
Regards,
Stephan