This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM64B: Problems to power on and boot up

Part Number: SK-AM64B

Hi everyone,

We bought some AM64B boards and followed this tutorial to get used to the board:

https://software-dl.ti.com/processor-sdk-linux/esd/AM64X/08_02_00_23/exports/docs/system/Demo_User_Guides/Benchmark_Demo_User_Guide.html

But it doesn't turn on or boot, we've tried other boot orders (with the board unplugged from any power source) but it just doesn't work. What concerns us the most is that even with 15W of power from a reliable sourc, the switch in the board on, and ethernet cables connected to routers on both NICs, we have no signs on the NICs LEDs, which is very odd since at least the power LED on either of the NICs (the orange one) should have shown some sign of life to us, which never happened.

When we use minicom or do a dmesg, it recognizes that exists a USB connection to a serial port (UART), but it is disconnected and never changes its state. We installed the Ubuntu 18.04 bare metal on a machine too, along with the devkit, and configured uboot and everything, but with no success either.

How can we make this thing work?