Up to now I was using the default GEL file for my board (DSK6713.gel). Now I have to make some modifications to the GEL file (different memory mapping) and I'm wondering if it is possible to specify a GEL file for my project that "overwrites" the default one.
Of course I could add a new configuration to the system setup with a different GEL file. But this is not so nice because the modifications are project specific.
Thanks for your help!
Robert