I want to simulate SuperSpeed using the IBIS model on the AM5728. Which ModelSelector should I use for SuperSpeed for the target pin?
AC11 USB_TXN0 Selector_3 0.16771 2.41602E-09 4.75415E-13
AD11 USB_TXP0 Selector_6 0.173562 2.8275E-09 4.57844E-13
Model Selector
Model_190 3-STATE,1.1V,USB3_TX_FS_NO_DEEMPHASIS
Model_191 3-STATE,1.1V,USB3_TX_FS_3p5_DEEMPHASIS
Model_192 3-STATE,1.1V,USB3_TX_HS_NO_DEEMPHASIS