Part Number: TDA4VM
Other Parts Discussed in Thread: ADS127L01, ADS8688
Hi team,
TDA4VM + ADS8688+ADS127L01 is being used. All data are captured through SPI under Linux.
Data acquisition through SPI communication under Linux is a bit inefficient and the customer requires at least 50K data acquisition frequencies, but currently only 10K. May I know is there a way to increase the frequency of data acquisition?
The ADS8688 is driven by the ti-ads8688 driver built into the Linux kernel, which captures data from the read and write drive files, and the ADS127L01 captures data through /dev/spidevx.x for SPI communication.
Could you help look into this case? Thanks.
Best Regards,
Cherry