Part Number: AM5748
Other Parts Discussed in Thread: ADS8598H
I intend to use AM5748 based SoM for a data acquisition and control system.
My primary requirement is to acquire data from a high speed 24 bit ADC ( 4x4ch = total 16 channels) at an interval of 10uS using the SPI communication ( I need to collect at least 100 K samples /s). Planning to select an ADC with data output rate of 500 ksps.
Also, the system should have USB and ethernet communication to communicate with the external devices.
I am planning to use the ARM core (linux kernal) for the external communication via USB/ethernet, PRU core for the data acquisition and shared memory for data exchange.
Please suggest this architecture meets my requirement.
As I mentioned earlier, I need to use SPI communication and whether I can connect to the same McSPI pins of AM5748 for establishing the communication and collecting data from the ADC using PRU or Do I need to use dedicated PRU pins for the same?