This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-TDAX: Image flipping

Part Number: PROCESSOR-SDK-TDAX


In TDA4 context, we need to flip the received image (from MIPI CSI-RX 0) either vertical or horizontal for the application. It is a 8bpp 3.2Mbits picture 30fps. 

Could you pls. share information here on how to do it using the Hardware accelerators ? 

We use TIOVX framework for capturing.  

Also, we need to calculate the CRC (CRC16) over the image buffer to verify the integrity of the image received from the Imager. Does CRC calculation can be delegated to any of the on-board accelerators to avoid CPU dependency ? 

kindly share your inputs. Thanks !