This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: C7X: Can't get simple memcpy to work with DmaUtilsAutoInc3d API

Part Number: TDA4VM

Hi,

I'm trying to migrate from vision_apps/appUdmaUtils to DmaUtilsAutoInc3d. I'm trying to get a memcpy working on the C7X using DmaUtilsAutoInc3d API. I basically reproduced a simplified dmautils_autoincrement_example.c.

My code does not hang or return errors, but I cannot get the DMA to actually copy into my destination buffer. This is confirmed by timing the time it takes to call DmaUtilsAutoInc3d_trigger() and DmaUtilsAutoInc3d_wait(). Whatever the buffer size, it's always 1us.

I assume it's some sort of virtual vs. physical address or cache stuff, but it might just be bad TR config. Here's the test code:

Fullscreen
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
#define REQUIRE(x) \
do { \
if (!(x)) \
{ \
VX_PRINT(VX_ZONE_ERROR, "Failed at { " #x " }\n"); \
return false; \
} \
} while (false)
static inline size_t Align(size_t val)
{
constexpr int DMA_ALIGN = 128;
return ((val + DMA_ALIGN - 1)/DMA_ALIGN) * DMA_ALIGN;
};
bool TestMemcpy()
{
// Setup DmaUtilsAutoInc3d_InitParam
//==================================
constexpr int N_CHANNELS = 1;
XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

What am I missing?

Thanks,

Fred

  • Hi Fred,

            Can you confirm if standalone dmautils test example is working at your end? I am suspecting that CLEC is not programmed correctly to route DRU events to c7x.

    Regards,

    Anshu

  • Hi Anshu,

    Thanks for the reply. I managed to build the dmautils_autoincrement_testapp for the C7X:

    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    11
    12
    root@ce56bf3ae428:/opt/ti-processor-sdk-rtos-j721e-evm-08_06_00_12/pdk_jacinto_08_06_00_31/packages/ti/build# make -s dmautils_autoincrement_testapp_freertos BOARD=j721e_evm CORE=c7x_1
    # Compiling j721e_evm:j721e:c7x_1:release:dmautils_autoincrement_testapp_freertos: main_rtos.c
    # Compiling j721e_evm:j721e:c7x_1:release:dmautils_autoincrement_testapp_freertos: dmautils_autoincrement_example.c
    # Compiling j721e_evm:j721e:c7x_1:release:dmautils_autoincrement_testapp_freertos: dmautils_autoincrement_test.c
    # Linking into /opt/ti-processor-sdk-rtos-j721e-evm-08_06_00_12/pdk_jacinto_08_06_00_31/packages/ti/binary/dmautils_autoincrement_testapp_freertos/bin/j721e_evm/dmautils_autoincrement_testapp_freertos_c7x_1_release.xe71...
    #
    <Linking>
    #
    # /opt/ti-processor-sdk-rtos-j721e-evm-08_06_00_12/pdk_jacinto_08_06_00_31/packages/ti/binary/dmautils_autoincrement_testapp_freertos/bin/j721e_evm/dmautils_autoincrement_testapp_freertos_c7x_1_release.xe71 created.
    #
    # Generating stripped image into /opt/ti-processor-sdk-rtos-j721e-evm-08_06_00_12/pdk_jacinto_08_06_00_31/packages/ti/binary/dmautils_autoincrement_testapp_freertos/bin/j721e_evm/dmautils_autoincrement_testapp_freertos_c7x_1_release_strip.xe71...
    #
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

    I'm not sure what to do with the .xe71, though. I'm used to building vision_apps and uploading vx_app_rtos_linux_c7x_1.out to /lib/firmware/vision_apps_evm. Is the .xe71 usable as a .out?

  • Hi,

        You can directly load .xe71 binary via CCS and run. You can refer the following document for the same : 

    https://software-dl.ti.com/jacinto7/esd/processor-sdk-rtos-jacinto7/08_06_01_03/exports/docs/psdk_rtos/docs/user_guide/ccs_setup_j721e.html


    Regards,

    Anshu

  • I don't have CCS setup and last time I tried following the "Debugging with HLOS running on A72", it did not go well. 

    I suppose then that the next best solution is to just copy the example in vision_apps' build system.

  • Hi,

        I see that you are using constexpr int CHANNEL_ID = 4; can you try by setting this to 0?


    Regards,

    Anshu

  • Same, output buffer is still filled with zeros

  • Hi Fred,

    I see that you are passing the below to the DMA 

    void* src = tivxMemAlloc(Align(IMG_SIZE), TIVX_MEM_EXTERNAL);

    void* dst = tivxMemAlloc(Align(IMG_SIZE), TIVX_MEM_EXTERNAL);

    Could you please printout these addresses? If it is something like 0x1 0xxx xxxxH then this would be the virtual address of the C7x. You would have to convert this to the physical address which would be something like 0x8 80xx xxxxH 
    You could convert this using the below function and pass the physical address to UDMA.

    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    11
    12
    13
    14
    15
    16
    /* Offset to be added to convert virtual address to physical address */
    #define VIRT_PHY_ADDR_OFFSET (DDR_64BIT_BASE_PADDR - DDR_64BIT_BASE_VADDR)
    uint64_t appUdmaVirtToPhyAddrConversion(const void *virtAddr,
    uint32_t chNum,
    void *appData)
    {
    uint64_t phyAddr = (uint64_t)virtAddr;
    if ((uint64_t)virtAddr >= DDR_64BIT_BASE_VADDR)
    {
    phyAddr = ((uint64_t)virtAddr + VIRT_PHY_ADDR_OFFSET);
    }
    return phyAddr;
    }
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

    Regards,

    Nikhil