Hi Ti experts
Does AM62Ax support eMMC HS400 mode? From the datasheet, it only mentioned HS200.
But from the AM62A-TRM, it also mentioned HS400. If the AM62A support HS400 mode, which Pin will be the DS?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ti experts
Does AM62Ax support eMMC HS400 mode? From the datasheet, it only mentioned HS200.
But from the AM62A-TRM, it also mentioned HS400. If the AM62A support HS400 mode, which Pin will be the DS?
AM62Ax does not support HS400. The MMC host controller supports HS400, but the MMC PHYs implemented in this device does not support HS400. The TRM should have an entry in the not supported section of the MMC chapter that says HS400 is not supported.
Regards,
Paul