This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

driver

Guru 13485 points

Other Parts Discussed in Thread: THS8200

Were I can find drivers for THS8200

  • Eli,

    Depending on how the THS8200 is connected specific drivers may not be needed as such.

    If the THS8200 is connected and configured as a generic RGB DAC and the syncs are passed directly from the DSP through level shifters then only a simple initialization is required, with all other configuration done through fbdev timing settings as per the generic 24 bit digital RGB DVO output.

    Bottom line, we do not have a specific driver since it depends very much on how the THS8200 is connected.

    BR,

    Steve

  • Hi,

     

    We have used THS8200 on DM6467T over 16bit embedded sync mode. You can get the THS8200 driver for this mode from arago tree.

     

    Thanks,

    Brijesh Jadav

  • Hi,

    How I can contact arago?

    b.regards

    Eli

  • Hi,

     

    Please find it at below location.

     

    http://arago-project.org/git/projects/?p=linux-davinci.git;a=blob;f=drivers/media/video/ths8200.c;h=1bfe8ae46aca8c58b63b6381dc3c01356a1be70c;hb=DAVINCIPSP_03.21.00.02

     

    Thx,

    Brijesh Jadav

  • Hi,

    See below customer feedbac/questions:

    My application is using the THS8200 on the output of a Video Scaler. The output format can vary from 480p to 1080p and have also a lot of VESA output standards. The output of the THS8200 is for a "VGA" output of the Scaler on a 15p DB connector with RGBHV output. The Scaler output is YUV 30 bit wide + H, V, DE controls. So I need the color space converter and I assume that the output mode is VESA mode. Do I need to configure the DTG timing registers for every VESA Standard? The HV signals from the Scaler already have the correct timing. If I need to configure the DTG does TI have a set of settings for the VESA standards?

     Thanks in advance for your feedback

    Eli

  • Hi eli,

     

    We dont have VESA standard supported on this driver. You will need to program DTG to generate VESA mode output.

    I did not get how scalar output is connected to THS8200 over 30 bit interface. Scalar typically outputs YUV422 data on 16 bit interface.

     

    thanks,

    Brijesh Jadav

  • Eli,

    Try the settings below which set up the THS8200 as a generic DAC.  The CSC and CSM are enabled to convert from reduced range YCbCr to RGB.  In this mode of operation you should be able to bypass the THS8200 with the syncs and directly connect the scaler syncs to the monitor.

    This appears to produce correct RGB levels as long as DE is not required to force a blank/black level.  This should be OK as long as the scaler is outputting correct black levels for YCbCr during blanking.

    //THS8200 Generic DAC setup
    WR_REG,THS8200,0x01,0x03,0xC1 // chip_ctl           
    WR_REG,THS8200,0x01,0x1C,0x70 // dman_cntl       24/30-bit input   
    WR_REG,THS8200,0x01,0x38,0x07 // dtg_mode      VESA mode DTG off      
    WR_REG,THS8200,0x01,0x82,0x1B // pol_cntl   DE disabled      

    //CSC Setup

    WR_REG,THS8200,0x01,0x04,0x81 // csc_ric1           
    WR_REG,THS8200,0x01,0x05,0xD5 // csc_rfc1           
    WR_REG,THS8200,0x01,0x06,0x00 // csc_ric2           
    WR_REG,THS8200,0x01,0x07,0x00 // csc_rfc2           
    WR_REG,THS8200,0x01,0x08,0x06 // csc_ric3           
    WR_REG,THS8200,0x01,0x09,0x29 // csc_rfc3           
    WR_REG,THS8200,0x01,0x0A,0x04 // csc_gic1           
    WR_REG,THS8200,0x01,0x0B,0x00 // csc_gfc1           
    WR_REG,THS8200,0x01,0x0C,0x04 // csc_gic2           
    WR_REG,THS8200,0x01,0x0D,0x00 // csc_gfc2           
    WR_REG,THS8200,0x01,0x0E,0x04 // csc_gic3           
    WR_REG,THS8200,0x01,0x0F,0x00 // csc_gfc3           
    WR_REG,THS8200,0x01,0x10,0x80 // csc_bic1           
    WR_REG,THS8200,0x01,0x11,0xBB // csc_bfc1           
    WR_REG,THS8200,0x01,0x12,0x07 // csc_bic2           
    WR_REG,THS8200,0x01,0x13,0x42 // csc_bfc2           
    WR_REG,THS8200,0x01,0x14,0x00 // csc_bic3           
    WR_REG,THS8200,0x01,0x15,0x00 // csc_bfc3           
    WR_REG,THS8200,0x01,0x16,0x14 // csc_offset1        
    WR_REG,THS8200,0x01,0x17,0xAE // csc_offset12       
    WR_REG,THS8200,0x01,0x18,0x8B // csc_offset23       
    WR_REG,THS8200,0x01,0x19,0x15 // csc_offset3        

    //CSM setup to map reduced range YCbCr to FS RGB        
    WR_REG,THS8200,0x01,0x41,0x40 // csm_clip_gy_low    
    WR_REG,THS8200,0x01,0x42,0x40 // csm_clip_bcb_low   
    WR_REG,THS8200,0x01,0x43,0x40 // csm_clip_rcr_low   
    WR_REG,THS8200,0x01,0x44,0x53 // csm_clip_gy_high   
    WR_REG,THS8200,0x01,0x45,0x3F // csm_clip_bcb_high  
    WR_REG,THS8200,0x01,0x46,0x3F // csm_clip_rcr_high  
    WR_REG,THS8200,0x01,0x47,0x40 // csm_shift_gy       
    WR_REG,THS8200,0x01,0x48,0x40 // csm_shift_bcb      
    WR_REG,THS8200,0x01,0x49,0x40 // csm_shift_rcr      
    WR_REG,THS8200,0x01,0x4A,0xFC // csm_mult_gy_msb    
    WR_REG,THS8200,0x01,0x4B,0x44 // csm_mult_bcb_rcr_msb
    WR_REG,THS8200,0x01,0x4C,0xAC // csm_mult_gy_lsb    
    WR_REG,THS8200,0x01,0x4D,0xAC // csm_mult_bcb_lsb   
    WR_REG,THS8200,0x01,0x4E,0xAC // csm_mult_rcr_lsb   
    WR_REG,THS8200,0x01,0x4F,0xFF // csm_mode           

  • Hi Tary,

    This setup Does not output Hsync and Vsync from the chip. Customer added a bypass wire to have the syncs to the output buffer.

    Is it possible to have the output pins working with only passing the input to output ? IS it possible to have the syncs output with the added delay of the internal process of the DAC + CSC + CSM ?

  • Eli,

    The THS8200 does not have a simple sync bypass mode where the inputs syncs pass through the THS, with delay matching.  The THS8200 sync polarity and widths must be uniquely programmed for each graphics format, however the process delay will be constant for all formats.  Attached is a setup file which includes numerous 30-bit graphics setups.  Thjis files has common settings and unique settings requrried for the various formats.

    Regards,

    Larry

     

    tvp7002_ths8200_evm_kit_081611.zip