This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: AM625 Secure CPU features

Part Number: AM625


Hi,

Can you please clarify the additional features which are available in the Secure version of the AM62x CPU P/N: AM6254ATCGHAALW which are not included in the Non-Secure CPU P/N: AM6254ATCGGAALW variant?

From the CPU datasheet it is not clear if the difference between the two parts is only secure boot or it includes other features.

Thanks,

Jhon

  • Hello Jhon,
    The difference between the two variants is on security features, specifically the feature listed under "Security" on P2 of AM62x datasheet is available only on AM62x security variant. One exception is Crypto HW block is also available on non-security variant.
    Best,
    -Hong