What problem it maybe ???? But i can connect XDS110 USB successfully.
1.
OS:Windows10
CCS:12.3
target:XDS 560 V2 STM USB,AM62A_SK_EVM;
2.
[Start: Spectrum Digital XDS560V2 STM USB Emulator_0]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\26300121\AppData\Local\TEXASI~1\
CCS\ccs1230\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'sd560v2u.out'.
E_RPCENV_IO_ERROR(-6) No connection: DTC_IO_Open::dtc_conf
Download failed for file D:\ti\ccs1230\ccs\ccs_base\common\uscif\xds560v2.out
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.

800
The explanation is:
An attempt to access the debug probe via USCIF ECOM has failed.
[End: Spectrum Digital XDS560V2 STM USB Emulator_0]