Other Parts Discussed in Thread: CCSTUDIO
I tried creating a new CDB file for my 6747 project and when it tries to translate it to TCF format I get an error in the DOS window (see below)...
When I looked for the folder:
c:/ccstudio_v3.3/bios_5_33_03/packages/ti/bios/config/update/5.25.06/
I noticed that .../update/5.25.06/ does not exist, instead I found:
...update/4.90.270 and
...update/4.90.280
I can only assume I did not install something properly.
Any ideas?
-howy
Running "C:\mic\qrx\Source\cdb2tcf.bat"
Please wait . . .
Conversion FAILED. This is the command execution log:
Application: C:/mic/qrx/Source/QRX_6747_b.cdb
Error: Seed file c:/ccstudio_v3.3/bios_5_33_03/packages/ti/bios/config/update/5.25.06/c6747.cdb cannot be found
Check if the directory c:/ccstudio_v3.3/bios_5_33_03/packages/ti/bios/config/update/5.25.06 exists.
If not, unzip the file update.zip, available in 'update' directory and try again
Error code 20
cdb2tcf command FAILED.
Press any key to continue . . .